This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB3410: Using TUSB3410 with an external oscillator.

Part Number: TUSB3410

Hello,

I'd like to use TUSB3410 with an external oscillator. (not crystal)

I have following questions.

1. How do we choose  between 1.8V internal regulator and external 1.8V power source? Is there any risk using internal regulator? (Some reference design using internal one, but some using external voltage divider.)

2. It seems that 1.8V 12MHz oscillator should be used, could you please tell me recommended voltage range of  X1/CLKI using 1.8V oscillator?  (Min & Max of Vih, Min and Max of Vil)

Best regards,

A.Sakai