Other Parts Discussed in Thread: BEAGLEBOARD-X15, , AM5728
Tool/software: Linux
Dear sir
We are developing the board with reference to the BeagleBoard-X15 board.
However, the TUSB8041 recognition problem faced a difficult situation.
When the power is turned on, the TUSB8041 recognizes the USB 2.0 mouse, and sometimes it does not recognize it.
In this case, measuring the USB VBUS voltage will measure + 0.6V .If it is recognized normally, + 5.0V is measured.
We can not find out what causes this problem.We attach the schematic we designed.
I look forward to your reply.
Best regards,
skbang
2746.SCHEMATIC1 _ p12_AM572x USB POR1.pdf5444.SCHEMATIC1 _ p76_USB HUB.pdfSCHEMATIC1 _ p77_AM5728_USB1.pdf