Hello
I am designing RS-422 interface circuit and RS-485 interface circuit using ISO1432.
Regarding the power supply to ISO1432, I am considering the following two cases, but let me confirm that there is no problem with the operation of ISO1432 in either case.
<Case1> VCC1 = 5V, VCC2 = 3.3V
<Case2> VCC1 = 3.3V, VCC2 = 5V
Regards,
MESH