This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7763: ADUM7643 Cross

Part Number: ISO7763

Hello, 

I am working to cross the ADUM7643, and I think the best cross is the ISO7763. Could you please help to confirm? 

Additionally, what is the biggest advantage of the ISO7763 over the ADUM7643? 

Best, 

Derek

  • Hi Derek,

    Thank you for posting to E2E!

    ISO7763 is the best cross we have to offer over ADuM7643 at this time, and it features higher isolation ratings, supports higher data rates (up to 100Mbps), it offers a wider ambient operating temperature range, and it can be powered by voltage supplies as low as 2.25V.

    Please let us know if there are targeted specifications you would like to compare.


    Thank you,
    Manuel Chavez