Part Number: ISO6740-Q1
Other Parts Discussed in Thread: ISO6740, ISO7741, ISO7710
Hi,
I am searching for an digital isolator where i can tristate outputs whenever required from the input side. ISO6740-Q1 has enable EN2. Is EN2 referenced to VCC2? VCC1 is 3.3V and VCC2 is 5V for my design. If EN2 is referenced to VCC2, I cant drive it from my FPGA which is working on CMOS3V3 logic. In this case, are there any digital isolators where i can tristate outputs from input side?
Thanks,
Srivatsa