This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] [H] Frequently Asked Questions: Isolation



Select this link to see answers to common questions, detailed use case implementations, and part recommendations for isolation devices.   
 
 
                                                                                                                                                 .     


Top Isolation FAQs - All-Time


What is the difference between ISOxxxxF and ISOxxxx devices (Ex. ISO7741 vs. ISO7741F)?

How to calculate the maximum SPI speed supported by a digital isolator?

Why is the logic LOW level output voltage, VOL1, up to 0.8V on Side 1 of the ISO1540 and ISO1541 bidirectional I2C isolators?

Can unused channel pins on a digital isolator be left floating?

How do you generate isolated power for an RS-485 node?

Can I power the two sides of a digital isolator with different voltages?

How do I read TI's Digital Isolator part numbers?

How to connect SPI MCU to multiple isolated SPI nodes?

SN650B-Q1: Driving waveform distortion at high temperature

PSPICE-FOR-TI: Adding a Library to PSPICE

Transformer Drivers: Frequently Asked Questions


Use the links below to find an answer to your question. If your question is not answered, feel free to post a question in our E2E forum. 

Digital
Isolators

Isolated 
Interfaces

Signal Isolators with Integrated Power

Opto-Emulators

Electromagnetic
Compatibility

Part Recommendations and Technical Training

High-Voltage Isolation
Parameters

Quality, Reliability,
and Certifications