Other Parts Discussed in Thread: SN6507, SN6501, SN6505B
Hi,
I have designed an isolated PSU based on SN6507 just to step up +5V to +12V.
The SN6507 is configured as follows:
Slew Rate:218 V/us
fCLK:575KHz
Current Limit - 1.2A
DC pin N.C - sets duty cycle to default 48%
Soft Start set to 9ms
The SN6507 connects to a pulsed transformer( ratio 3:8 ; primary inductance of 300uH; Vit= 11V/uS) and rectifier diodes MBR0580S1-7. Also have snubbers at the secundary.
The load is a TI device with an internal LDO regulator. I have seen the output rail that powers this device to be 14.4V when the device is operating. This is slightly higher than expected (it should around 13.3V, the 5V input is very accurate). However, when this device is in sleep mode it only draws 100uA, when this is the case I see the rail going up to ~24V.
Is this a saturation of the transformer ? is it caused by virtually no current drawn by the load?
I have added a zener to clamp the rail , but I do not want to rely on that only, and at the same time I was a simple and cheap solution. Should I add a pre load, to ensure a min current is always drawn say 1mA, would that help the SN 6507? Datasheet does not provide much guidance?
Thanks in advance