Hello,
I admire your isolators, for example iso6731.
You offer two version of the "default output": High or Low (F suffix).
So you need to manufacture double the number of models,
distributors need to keep double space on their shelfs,
users may suffer double trouble like me now
(in one project I need both versions, hence one tape more at smd placement).
On page 23 I see that it is just a one 1.5 Meg pulled up or down.
On page 3 we have two unconnected pins 6,11.
So the question seems to be obvious:
why not to allow the user to decide and connect this 1.5Meg resistor (up/down) via these pins?
And reduce the mess by half?
Best regards
Robert