Part Number: ISO1541
Other Parts Discussed in Thread: ISO1540, ISO1640, ISO1641

+
. Side1: VCC1-3.3V , GND1 -GND
. Side2: VCC2-5V , GND2 -PGND
check with the schematic diagram, we are not able to communicate two devices via ISO1541
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Thank you for your inquiry.
There are a few points I would like to make regarding the information you have provided:
There are also a few questions I would like to ask:
Regards,
Aaditya Vittal
Thank you for the replay,
as for your review, I will add the 0.1Uf on the side also then I will try
I am using isolation I2C for the SM BUS commutation. with STM32F104 and the side1, I am connecting to the STM and Side2 connecting SMBUS device.
whatever the given wave is for is Side2, in Side I made a master to request data from the 02 address, The STM I set is 02 address but I am not getting any replay for the STM model, without ISO1541 it's working fine.
Hello Gopal,
Thank you for the additional details, I do not see any with the connections you mentioned.
Please add the 0.1uF capacitor since it is required for normal operation. Let us know if the problem continues.
Best,
Andrew