Part Number: ISO1228
Other Parts Discussed in Thread: ISO1212, , ISO1211, ISOM8110, ISOM8710
Tool/software:
Hi!
I'm thinking about using the ISO1228, ISO1211 or ISO1212 in one design. In ISO1228 datasheet the maximum operating condition says that the maximum sink/source is about 3.3/4.2mA, but my application requires a minimum current of 10 - 20 mA because that is the current that the load device will consider as active state (the other side of the device in the field side is a high-side switch with a current proportional feedback pin with a large attenuation factor).


Could I add some external components to the ISO1228 to increase the maximum source/sink current per pin?
Maybe this is not the best IC for my application, I would appreciate any comments.
Thank you very much in advance.