Part Number: LM5180
Tool/software:
Hi. using LM5180 dual out put
Transformer design Nps = 1.2 , Lm = 40uH
Output Voltage = 20V , 0.1A
When Rfb = 300K and Rset = 16K, the output voltage is 20V. Is it possible to change Rset to 12.1K? Will there be any issues if I change Rset? Additionally, when I measure the voltage at Rset with a multimeter, the IC stops functioning. Is there no way to measure the voltage at Rset?
My circuit