This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO6520: Is this part able to be used for two PWM signals?

Part Number: ISO6520


Tool/software:

Hello friends!

I am looking for a digital isolator for use with two PWM signals that need isolation and I've found the ISO6520DR. Because I am dummy in isolation ICs, please, could you confirm me that this part is good to be used with PWM signals?

Edit: The two PWM signals are going to be used for low power servo motor control.

Many thanks in advance!

Br,

Luis