ISO1640: I2C rise time is too long and input signal wave issue

Part Number: ISO1640
Other Parts Discussed in Thread: PGA900

Tool/software:

Hi:

I use ISO1640 as I2C output isolator for PGA900.

But I find I2C SDA rise time is too long. PGA900 SDA rise time is about 240ns without IS01640 in 400KHZ.

But when I connect the PGA900 i2c to ISO1640, the rise time will be 360ns that is longer than 300ns.

I find there is strong wave on input SDA signal ,like the picture, there is 110ns flat wave part which make the rise time be longer than 300ns.

How can I reduce the rise time?

I have try to change R3 R5 from 100OHM to 0ohm but helpless for this issue.