Other Parts Discussed in Thread: ISO35T, , ISO1410, ISO35
We use the ISO35T with a coilcraft transformer.
Which advantages/disadvantages would it have to instead use the ISO1500 or ISO1410 with isolated control of the transformer?
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alen,
Please do note that ISO35T is an isolated RS-485 transceiver with an integrated transformer driver while ISO1410 and ISO1500 are the isolated RS-485 transceivers which do not integrate any transformer driver. This means that you would require an external transformer driver like SN6505 to generate isolated power.
Apart from the above difference, ISO1410 and ISO1500 devices are our latest isolated RS-485 transceivers with many advantages over ISO35T. Please find below some of advantages that the two devices have over ISO35T.
In addition to the above benefits, ISO14xx family of devices offer the below advantages as well.
Between ISO14xx and ISO1500, the ISO14xx family of devices supports reinforced isolation while ISO1500 supports basic isolation & is available in a much smaller package which is suitable for cost sensitive application. Thanks.
Regards,
Koteshwar Rao