This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7041: Similar part with 1.8V supply

Part Number: ISO7041
Other Parts Discussed in Thread: ISO7021

Hi team,

I checked the ISO7041 supports 2.25 V to 5.5 V supply voltage, could you recommend a similar part with 4-channels support 1.8V supply voltage?

Thank you.

Regards,

Allen

  • Hi Allen,

    Currently we do not have a 4-channel device that supports 1.8V operation but we did release a 2-channel device ISO7021 that supports 1.8V, 2.5V, 3.3V & 5V operation. I will also reach out to you over email to understand more about the requirement. Thanks.

    Regards,
    Koteshwar Rao