Part Number: ISO1410
Hi everyone,
We are working with the ISO1410 half-duplex RS485/RS422 transceiver in our latest design. We are sending data on D line using a USB - UART interface module, when REb is low, DE is high. However we are unable to observe any data on the A and B lines. Following is the portion of schematic where we use the transceiver. R7, R9 and R10 are zero-ohm resistors while C14, C15 and C20 are DNMs.
Could someone suggest what can be going wrong here?
Thanks in advance,
-Chandrasekhar DVS