This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi everyone,
We are working with the ISO1410 half-duplex RS485/RS422 transceiver in our latest design. We are sending data on D line using a USB - UART interface module, when REb is low, DE is high. However we are unable to observe any data on the A and B lines. Following is the portion of schematic where we use the transceiver. R7, R9 and R10 are zero-ohm resistors while C14, C15 and C20 are DNMs.
Could someone suggest what can be going wrong here?
Thanks in advance,
-Chandrasekhar DVS
Chandrasekhar DVS,
I'm sorry you're having this issue. I think I see the problem though.
The ISO1410 is a half duplex device in the ISO14xx family and the pinout is different on the bus side from the full duplex versions. I see you have the symbol for the full duplex devices in the schematic which means the bus lines aren't connected to the correct pins of the device.
Respectfully,
Lucas Schulte