This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7740: the NC pin for ISO7740

Part Number: ISO7740


hi 

can I keep connect NC to gnd or NC to vcc.

does it cause ISO7740 abnormal ?

  • Hi Dimitry,

    The NC pin of ISO7740 is internally not connected, hence, it doesn't matter whether you connect it to GND or VCC. If it is an option to leave it open / floating then probably that would be best. Thanks.

    Regards,
    Koteshwar Rao