Hi Team,
My customer plan to use ISO7740 enable pin. VCCI = 3.3V, VCCO=5V.
We have questions, when giving 3.3V to enable pin, is the output normal?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
My customer plan to use ISO7740 enable pin. VCCI = 3.3V, VCCO=5V.
We have questions, when giving 3.3V to enable pin, is the output normal?
Thanks!
Hi Eggsy,
Thank you for posting to E2E! HIGH level inputs to the ISO77xx are defined as a ratio of > 0.7 x VCCO. For VCCO = 5V, 3.3V is just below this threshold (3.5V) so not guaranteed for normal output. However, since the Enable pin is active by default, the ISO7740 output will be normal whether EN = VCCO or is left floating.
Is our customer able to leave the Enable pin floating instead of connecting 3.3V?
Thank you for your time,
Manuel Chavez
PSA: Post edited to clarify that the ISO77xx Enable pins are active by default
Hi Manuel,
Thanks for your help!
Customer need use EN pin, they will PD EN pin by default. When MCU ready, they will let EN pin go high.
Hi Eggsy,
Is there a way our customer can turn the pin off instead of sending the 3.3V "HIGH" signal? A 5V HIGH signal is preferred, but an internal pull-up resistor can connect enable to VCCO if the pin is disconnected or high impedence.
Please let me know,
Manuel Chavez