I know theTMS470R1B1M status is NRND, Now I just maintain old project which was done by the former engineer. Since he had left, so I only have a limited document about that project.
I use Jlink 4.98a + Jlink V8, in J-Flash IDE.
I load TMS470R1B1M.jflash firstly, and try to connect the chip, Unfortunately, getting the error as "could not detect CPU clock speed" or " 'Memory access timed out @ 0040FFE0 ".
when I use J-link commander, it can automatically identify the chip ID, but I can 't take any further commander, getting the error as " Not able to access the RAM/FLASH".
so would you please give me some suggestion about how to program the TMS470R1B1M.
Thanks very much.
PS: AWD connect to the ground by 10K resistance.