We're using the TPS40170-EP in a 12V->5V application.
I've added an overvoltage protection crowbar to the output, which short circuits the regulator output if an over-voltage condition is detected (e.g. in case of a faulty VFB network)
The expectation is that the TPS40170 will shutdown and attempt its soft-start cycle each time the crowbar triggers. The crowbar is limited to 0.2A continuous (i.e. it can survive the initial short-circuit current, but relies on the TPS40170 OCP to stop to prevent large continuous currents from flowing.
At Vin>11V the circuit works correctly - the crowbar trips, causing a short on the regulator output, and this causes the TPS40170 to enter a reset mode, with 100ms cycle time between attempts (soft-start mode)
At Vin<11V tripping the crowbar causes circuit oscillation. The TPS40170 attempts to restart immediately after each over-current condition (<100us) (e.g. cycle by cycle?) - and this causes overheating of the crowbar circuit.
Is there any way to ensure that the TPS40170 goes through the full power on reset after a short circuit fault (My crowbar can only pull down to 0.8V guaranteed)?