Hello!
I use LMH6702QML (5962F0254602VPA) in my design. I have a requirement that no free pin be floating. Can I connect pins 1, 5, 8 (N / C) to the ground (power supply minus) or to the power supply plus?
Regards
Ilya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello!
I use LMH6702QML (5962F0254602VPA) in my design. I have a requirement that no free pin be floating. Can I connect pins 1, 5, 8 (N / C) to the ground (power supply minus) or to the power supply plus?
Regards
Ilya
Hello Ilya,
The N/C pins are not internally bonded and are floating. If these pins are connected on a board, it is typically to ground but there should be no issues with connecting them to supply, other than having extra metal at the supply pontential.