This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM185QML: LM185BWG/883 - Need Reflow Profile

Part Number: LM185QML

Hello,

We have a customer asking for the recommended reflow profile for this device, it is not listed in the datasheet  (it simply says "Call TI").

Could someone please advise?

Thanks,

  • Hello Gabe,

    I am looking into this and hope to have a response for you sometime tomorrow.

    Thanks,
    Kyle
  • Hello Gabe,
    this is our standard reply on solder reflow.
    Note that the part in question does not have a metal lid so the third paragraph does not apply and it does not have gold plated leads, so the fourth paragraph does not apply either.

    • At the board level, solder reflow profiles are dependent on numerous factors including, but not limited to, solder type, flux, package type, number of components, board layers, board size, reflow oven type and accuracy as well as pre and post cleaning processes. Because of the number of variables it is not possible to provide a single reflow profile that is representative of every board using a specific package type. Typically manufacturing houses have reflow profiles in place and modify them for specific hardware.

    • TI suggests using the flux manufacturer’s recommended profile as a starting point. In general ceramic parts are compatible with ramp-rates of less than or equal to 5°C/second with a maximum temperature of 265°C. Variations of course need to be comprehended based on time required to volatize the flux prior to the solder reaching liquidus.

    • Metal lid packages use a 80%Au20%Sn gold-tin solder preform to attach the lid. Gold-tin solder will begin to soften at 270°C and has a eutectic point of 280°C. The package body temperature must not be allowed to exceed 265°C at any time or permanent damage will occur due to compromising the package’s hermetic seal. Note that though-hole hermetic device specify a maximum temperature for soldering as a lead-temperature of 300°C for 10 seconds. This is not a reflow temperature.

    • When using gold-plated leads or pads with MIL-SPEC plating thickness (60 µ-in to 225 µ-in), it is strongly recommended that the units be pre-tinned (solder-dipped) before board mounting to scavenge the gold from the leads or pads. If this is not done there is a chance of gold-embrittlement of the board-level solder-joints. A flowing solder-pot or two passes in a static solder-part is recommended.
  • Hi Kirby,

    Can you advise what the Lead ball finish would be for this and the 5962-9091402QYA (the finish also states, "Call TI".

    Thanks,
  • Hi Gabe,
    The lead finish is SnPb solder dip. (63% tin/37% lead)