This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC2201-SP: Power Rail Verification

Part Number: TLC2201-SP

Hi,

I'd like to verify the rails this part can operate from. It has an absolute maximum rating specified of +/-8V for the supplies and a maximum input voltage of 8V (to any input, with this referenced to the mid-point of the supplies).

Would I have any issues running this part off of a unipolar 12V supply?

Thanks