hi,
feedback resistors are calculated to 3.3V, but when power up the device there is overshoot to 3.6V and then dropping to 3.3V. the time from overshoot until stable is about 20uS
1. is this normal behaviour?
2. can i do anything to fix this?
the resistors I am using are 5.32K, 3.01K and compensation capacitor of 220pF.
I tried to increase the compensation capacitor to 820pF but no change.
please advise.
Thanks