Hi All,
We are planning to use TPS7H1101A-SP for our project with below specifications:
Vin = 5V
Vout= 3.5V
Iout = 2.376A
With these specifications total power dissipation comes out to be 3.564W.
In TPS7H1101A-SP datasheet RθJC = 0.6°C/W but RθJA is not given. Generally power disspation is calculated using RθJA.
So my question is how to calculate maximum power dissipation of TPS7H1101A-SP using RθJC.?
And can we use TPS7H1101A-SP with specifications mentioned above.