This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Aptina camera interface to VAYU VISION application board

Hi Team,

I have TI VAYU VISION application board with me, Here I would like to interface Aptina camera to board with the interface given on board. Currently I have Aptina MT9V024 camera with me. Here I would like to know it is possible to interface Aptina MT9V024 camera to the board or not? as the recommended camera for the board is Aptina MT9V022(P3) and OMNIVISION OV10630(P1).

FYI in am referring the board BSP user guide for the purpose. Please suggest, If any documentation or pin details for camera interface shared it will be much helpful.

Regards,

Rohit

  • Rohit,

    This thread has been moved to a more appropriate forum for support.

    Regards,
    Eric Hackett
  • Hi Rohit,
    What is your processor ?
    What is your OS ?
    Starterware or Linux or TI-RTOS etc., ?
  • Hi Rohit,

    Please mention the processor ( OMAPL1x ? or AM1X ? or C674X ? ) Is it a custom board or TI EVM?

    What is the BSP user guide you are referring?. It belongs to which processor ?

    If you are using the OMAPL1x, a composite Leopard Imaging camera is interfaced with the OMAPL138 LCDK board. you can refer to 

    Regards,

    Shankari

    -------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.
    --------------------------------------------------------------------------------------------------------

  • HI Shankari / Titus S,

    My board details are as follows:

    Processor : DRA7xx series (VAYU Board TDA2xx series)
    daughter board : VAYU VISION Application Board Rev C.
    OS : SYS/BIOS version bios_6_41_01_36
    Starterware_01_02_05_08

    I specifically want to know the pin details of P3 connector(Aptina camera) of the daughter board. FYI the recommended camera for this board is Aptina MT9V022(P3) but we have Aptina MT9V024. Just wanted to cross check the pin compatibility of our camera with board.

    Thanks & Regards,
    Rohit
  • Hi Rohit,
    I've looked into the both sensors MT9V024 and MT9V022 data sheet.
    It seems to be both are pin to pin compatible.
  • Hi Titus S,

    Thanks for your reply. Could you please share data sheet for both sensors MT9V024 and MT9V022 which your are referring to.

    Regards,
    Rohit
  • Hi Titus,

    Thanks you for your prompt reply and the information shared.

    The pin details of the Aptina (MT9V024) camera board (Black PCB in the uploaded image) has some details given. I don't see any pin details of the VAYU vision board Aptina connector, (Aptina P3). Just to make sure that I don't burn the boards due to pin mismatch (especially VCC abnd GND).  It would be great if we get some information of the pin to pin details of the P3 connector.

    Attached is the image of Aptina camera MT9V024 for your reference. Please suggest.

    Regards,

    Rohit

    Aptina_camera_pin_details.pptx

  • Hi Rohit,
    I'm not sure about P3 connector of VAYU vision board.
    Do you have schematics of this board ?
    Just I checked the both data sheets of camera.


    I specifically want to know the pin details of P3 connector(Aptina camera) of the daughter board. FYI the recommended camera for this board is Aptina MT9V022(P3) but we have Aptina MT9V024. Just wanted to cross check the pin compatibility of our camera with board.

    You said that MT9V022 camera would support VAYU vision board ?
    Where did you see this info about "MT9V022" that would support for this board ?
    If thats the case then it surely work well, no issues.
  • Hello Rohit,

    The VAYU vision board is based on OMAP5 application processor. So moving this thread to correct forum to get better response.

    Regards,
    Senthil
  • Hello Rohit,

    I have TI VAYU VISION application board with me, Here I would like to interface Aptina camera to board with the interface given on board. Currently I haveAptina MT9V024 camera with me. Here I would like to know it is possible to interface Aptina MT9V024 camera to the board or not? as the recommended camera for the board is Aptina MT9V022(P3) and OMNIVISION OV10630(P1).

    There is user guide for TDA2x  - VISIONSUPER28 – VISION APPLICATION BOARD. This document contains all supported features of TDA2x vision application board.

    This board supports Stand-alone camera module head boards - AR0132AT6C00XPEAH-E head board from Aptina

    I suggest you to contact your local FAE and request board schematic and user guide. I would not you that these documents are under TI NDA agreement.

    Best regards,

    Yanko