This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV244A: Please tell me about the case where the undershoot is below -0.5V.

Part Number: SN74LV244A

Hello.

Please tell me about the case where the undershoot is below -0.5V.
Not found on the datasheet.

If the input waveform is -0.5V or less, are there any relaxation conditions according to the time regulation?

For example
If the input voltage below -0.5V is 20ns or less, up to -1.0V is acceptable.
Such

Regurd,

 Hirofumi Yamaguchi