Part Number: CD4010B-Q1
Other Parts Discussed in Thread: TXU0104, SN74LXC8T245
I would like to use CD4010B-Q1 to translate digital lines from a 3,3V sensor to 5V uC
in The datasheet in the table "STATIC ELECTRICAL CHARACTERISTICS" there are VOL Max, VOH Min, VIL Max and VIH Min specified only for Vdd=5, 10 and 15V
in the "RECOMMENDED OPERATING CONDITIONS" Vdd is specified as at least 3V so I assume this IC can be used to translate 3,3V to 5V levels.
How to obtain values for VOL Max, VOH Min, VIL Max and VIH Min when Vdd=5V and Vcc=3,3V?
best regards
Arek