Hello E2E,
The datasheet mentioned that ESD Protection Exceeds 2000 V Per MIL-STD-883, Method 3015. Is this the human body model (HBM) ESD for SN74ABT16374ADGGR?
Regards,
Carlo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello E2E,
The datasheet mentioned that ESD Protection Exceeds 2000 V Per MIL-STD-883, Method 3015. Is this the human body model (HBM) ESD for SN74ABT16374ADGGR?
Regards,
Carlo
Hi Carlo,
Yes, this is referring to the HBM standard, which was defined in the US military standard MIL-STD-883, Method 3015, and is now internationally defined in JEDEC standard JS-001.