Other Parts Discussed in Thread: SN74LVC125A, PCA9306
Hi Sir,
My customer would like design SN74AVC4T774RSVR for I2S and PCA9306DCUR for I2C.
Would you please review schematic and layout and provide your comment?
BR,
SHH
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
My customer would like design SN74AVC4T774RSVR for I2S and PCA9306DCUR for I2C.
Would you please review schematic and layout and provide your comment?
BR,
SHH
The SN74AVC4T774, like any other logic device, needs decoupling capacitors at its supply pins.
For unidirectional downtranslation, a flexible lever shifter like the SN74AVC4T774 will work, but is overkill. You can simple use a buffer with overvoltage-tolerant inputs like the SN74LVC125A (see this list).
The PCA9306 circuit is wrong; VREF1/2 are not power supply pins. You can either use the slow switch configuration (connect EN directly to 1.8 V, leave VREF1/2 open), or the normal level shifter configuration (connect VREF1 directly to 1.8 V, connect VREF2 and EN together and through a 200 kΩ resistor to 3.3 V; SCA1/SCL1 is the low-voltage side). See the datasheet.
All four I²C signals need pull-up resistors; I assume they are present, but elsewhere on the schematic.
Hi Clemens,
thanks for feedback.
would you please review the updated PCA9306 scheamtic and let me know your comment?
BR,
SHH