This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
If the OE pin is high, does a through current flow even if the A pin has a high impedance?
Best regards
Goto
The A inputs always have high impedance (for allowed input voltages). The leakage current is specified as II and is independent of the state of the /OE pins.
When the OE pin is high, input a voltage between high and low to the A pin.
At this time, does a through current flow from the power supply to the ground inside the device?
The /OE pins disable only the outputs. For input voltages not at the rails, you will indeed get shoot-through currents.