Other Parts Discussed in Thread: SN74LVC06A, SN74LVC3G06
A customer has TXS0104ERGYR on their board, and they have a couple of LED’s on it’s port B, which is powered by 3.3V.
If a Port B output pin is high, what is the drive capability of that pin (when operating at 3.3V)?
I do note that TX0104ERGYR datasheet shows an absolute max continuous current of 50mA, but I don’t see a typical operating max current spec’d out. (And I’m not sure if chip is designed to last with a continuous load of say 10mA or not.)