Hello Team,
The maximum input leakage current of the SN74HCS02QPWRQ1 is mentioned as ±1000nA at Tamb=25°C. Whether this value is same at -40°C and at +125°C.
Because I am comparing this IC with SN74HC02QPWRQ1 for which, input leakage current is mentioned as ±1000nA at Tamb =125°C. But at Tamb= 25°C, same is only ±100nA (Max).
So only if I know the Input leakage current of first part at Tamb = 125°C, I can compare it with that of second part.
Thanks in advance.