This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For VCC=3V Vt+ max = 1.87V and Vt- min = 0.84V. What is Vt+ max and Vt- min for VCC=3.3V?
3 V is the worst case for a power supply with 3.3 V ± 10%.
If you really want vaues for exactly 3.3 V, see [FAQ] What method is best used for estimating specification values between those given in the datasheet?