Other Parts Discussed in Thread: SN74AHC14Q-Q1, SN74AHC14
Hi,
I'm trying to choose an alternative for one of the existing component in our designs. The existing component supports only -40°C to +85°C. I am considering SN74AHC14-EP or SN74AHC14Q-Q1 as an alternate.
The datasheet for SN74AHC14 mentions the VOL max data for -40°C to +85°C as 0.44V and -40°C to +125°C as 0.5V.
But the datasheets for SN74AHC14-EP and SN74AHC14Q-Q1 mention the VOL max only for -40°C to +125°C.
Since the SN74AHC14-EP and SN74AHC14Q-Q1 are enhanced products of SN74AHC14, do they have VOL max limited to 0.44V at -40°C to +85°C even though this temperature range specifically not mentioned in the datasheets? Could you please confirm?
Thank you,
Komal Charan Garlapati.