This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXU0204: Operating voltage

Genius 16630 points
Part Number: TXU0204

Hi Experts,

Customer is planning to use the TXU0204 to perform level conversion.

Is this correct in assuming that the following supply voltages can be used?

  • VCCA=1.2V,VCCB=1.2V
  • VCCA=1.8V,VCCB=1.8V

7.7 Switching Characteristics, VCCA = 1.2 ± 0.1V and 7.9 Switching Characteristics, VCCA = 1.8 ± 0.15V.

Regards,
Archie A.