This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHCT14: About Cpd specifications

Part Number: SN74AHCT14
Other Parts Discussed in Thread: SN74AHC14, SN54AHCT14, SN54AHCT14-SP, ,

Dear Team,

The Cpd of SN74AHCT14 is 112pF (typ).

However, the Cpd of a close series, SN74AHC14, is 9pF (typ).

I don't know the temperature conditions for SN74AHC14, but the other measurement conditions are listed as the same.

SN74AHC14: No load, f=1MHz, VCC=5V

SN74AHCT14: No load, f=1MHz, VCC=5V, TA=25℃

Could you tell me what is the reason for the difference between the values for both products?

Best regards,

Luna