This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD74HC4017-Q1: 10Hz to 1Hz decade divider with <130ns tpd over temperature

Part Number: CD74HC4017-Q1
Other Parts Discussed in Thread: SN74LVC574A-Q1, SN74LV393A-Q1, SN74LVC1G11-Q1

Hi team,

My customer is looking for a decade divider which has <130ns tpd over temperature.

The use case is a clock for V2X chip and need to divide 10Hz to 1Hz. VCC is 3.3V. And AEC-Q100 is required.

Could you suggest the best device which can achieve this requirements?

Best Regards,