This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0102: UART 1.8 to 3.3V Level shift with OE connecting with 3.3V PG signal

Part Number: TXS0102
Other Parts Discussed in Thread: TXU0202, SN74AXC2T245-Q1

a. I am going to use this part for UART 1.8V to 3.3V level shift. so VCCA -> 1.8V, VCCB -> 3.3V ( As per datasheet, VCCA<VCCB)

b. As mentioned in the datasheet, OE pin is referenced to VCCA (1.8), but in my design the OE pin will be connected with a PG signal which is 3.3V. 

c. In recommended operating condition, OE pin max is mentioned as 5V, so I guess this should not be problem, but I need confirmation.