Hi,
I want to know the maximum data rate supported by CLVC16T245MDGGREP IC.
Thanks in Advance
Ranjini
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to know the maximum data rate supported by CLVC16T245MDGGREP IC.
Thanks in Advance
Ranjini
Hello Ranjini,
The maximum data rate supported by the part is 200 MHz.
Kind regards,
Reed Smoot
Hi Ranjini,
Since the maximum frequency of 200 MHz is correlated to a voltage translation of 3.3 V to 5 V, theoretically a reduction to half of that voltage would correlate to half of that frequency.
However, to accurately determine the maximum data rate for 1.8 V to 3.3 V and vice versa, I recommend testing this part on an EVM with the specific output load of your application. This will be the only way to realistically verify the maximum data rate for your system.
Sincerely,
Reed Smoot