Part Number: SN74LVC2G17
Hello e2e team,
I am using the SN74LVC2G17 buffer in my design and connected the PWM inputs as follows via the pull down resistor 10k ohm -->

The issue is when I give the supply 3.3V, the pin 2 (of both J17 and J18) both are somehow pulled up (~2.3V) instead of getting tied by GND via pull down resistors. I see the PWM input wave going from 2.3V to 3.3V instead of 0 to 3.3V --> level shift.
Could you please tell me what could be the possible source of error here ? I even tried replacing the 10K resistor value with 1k and 100k but still no change.
Thank you,
Anubha