This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74ABT241A: Can this be used to safely drive an LED Cathode (Anode at 5.0 volts, Vcc at 5.0 volts)?

Part Number: SN74ABT241A
Other Parts Discussed in Thread: TPL7407LA

Will the output stage get damaged if the pin is pulled to a higher voltage than it's being driven to by the chip?  Also, will there be any current flow?

And if this isn't a good idea, any suggestions for a suitable cheap 5.0 volt, 64 mA hex or octal driver?

Thanks,

-Mike