SN74LVCC3245ADBR and CLVCC3245AIDBREP have similar specifications and packages, what are the differences?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SN74LVCC3245ADBR and CLVCC3245AIDBREP have similar specifications and packages, what are the differences?
The Enhanced Product Selection Guide says:
Our enhanced products portfolio mitigates the risks that the avionics and defense markets face with COTS integrated circuits (ICs) by:
- Using the latest and most robust plastic encapsulation methodology to support the harsh environment needs.
- Ensuring tin plating content is not above 97% to eliminate the risks related to time-dependent pin-to-pin metal shorts (aka tin whiskers) by assembling the device with NiPdAu plating or SnPb solder balls.
- Using only gold (Au) bond wires to ensure the highest quality die to leadframe connection.
- Performing extended 250 hours highly accelerated temperature and humidity stress testing (HAST) to demonstrate improved moisture resistance, extending both operational life and dormant storage capabilities.
- Extending temperature ranges from -55°C to 125°C to enable the broadest possible use cases.
- Ensuring a single controlled manufacturing baseline flow with a single wafer fab, assembly site and test site to ensure the applicability of customer’s qualification even over multi-decade programs.
- Ensuring orderable (V62/xxxx) DLA vendor items drawings part numbers that eliminate the need specification source controlled drawings.
thank you for your answer.
Does that mean there is no difference in electrical characteristics between SN74LVCC3245ADBR and CLVCC3245AIDBREP?