Hi Team,
Can the input voltage level exceed the VCC of SN74LVC1G17 ?
eg. When input 24V then on the green marked point the voltage is 3.9V ( 3.3V + Vf of the BAV99 diode).
Is this ok for SN74LVC1G17 ? In the case the A input is 3.9V will then the Y output of SN74LVC1G17 be 3.3V?
Best Regards,
D.