Hi Team
Could you please confirm whether my understanding to the input voltage tolerance range is correct? I found no specifications on datasheet but is expecting it to have the same range as Vcc.
Max: 7V
Min: -0.5V
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team
Could you please confirm whether my understanding to the input voltage tolerance range is correct? I found no specifications on datasheet but is expecting it to have the same range as Vcc.
Max: 7V
Min: -0.5V
Thanks
Hi David,
The speciifcation is in the recommended operating conditions table here:
Hi Emrys
Appreciate the response!
I'm aware of the recommended condition, but due to parasitic components at the input my customer is observing some voltage overshoots and undershoots, could you please help check if there's any specifications on absolute maximum ratings?
Regards
Hi David,
The inputs include positive and negative clamp diodes. The inputs can exceed the voltage rating (Vcc) so long as the current through the clamp diode is limited to 20 mA or less.