Other Parts Discussed in Thread: SN74LVC1G08, SN74LVC1G99
Hello TI experts,
My customer wants to apply different voltages to each input with SN74AUP1G08.
input B (pin1) : 4.0V
input A (pin2) : 1.8V
VCC : 1.8V
maybe output would be 1.8V when logic is high because VCC is 1.8V.
is it okay for this situation?
I cannot find any recommended maximum input voltage for logic high.
(I can find absolute maximum rating - it is 4.6V - but I think it is not recommended.)
please check this issue. Thanks.
Best regards,
Chase