Part Number: SN74HCT08
Other Parts Discussed in Thread: UCC23313, , SN74ACT08
Hi expert,
My customer use two SN74HCT08 driver 4 UCC23313, but since the current drive is not enough, the output voltage will drop to 4.2V with 5V VCC.
if they use one SN74HCT08 driver 4 UCC23313, the voltage will drop to 3.8V.
UCC23313 need 16mA at max, and customer test showed it need 8mA on each UCC23313.

So I suggest customer to use a high current AND gate,SN74ACT08, this is better and output voltage is 4.5V.
Question 1: And customer hope to understand why these two devices have difference on IOL and IOH.
Besides, they found the SN74ACT08 will eat some duty cycle.
When input is 5% and output is only 2% during soft start phase. Question2 :and they want to know what cause this phenomenon?
BR
Emma