This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108E: IO clamping when VCC = 0V ?

Part Number: TXS0108E

Hi All.

A quick question about the TXS0108E. Is it safe to drive the IO pins when there is no supply voltage on the VCC in question? Let's say that both VCCa and VCCb are at 0V but A MCU is driving the IO's pins high on side B Would that be safe or would the IO pins be clamped due to internal diodes that reference to the VCCb (0V) and then drag an undesired amount of current?

Thanks and have a nice day.