This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD40106B: error in PSpice for TI

Genius 12865 points
Part Number: CD40106B
Other Parts Discussed in Thread: CD4049UB, , CD4069UB

Hello Team,

I see the errors shown below when using the models CD40106B, CD4049UB, CD4069UB from PSpice for TI (without adding a model).

When will this be fixed in Pspice for TI, please? 

ERROR(ORPSIM-15141): Less than 2 connections at node X_U1.XU1.NA1.

ERROR(ORPSIM-15141): Less than 2 connections at node X_U1.XU1.NB1.

ERROR(ORPSIM-15141): Less than 2 connections at node X_U1.XU1.NO1.

Thanks and Best Regards, Hans